VFX artists refine character animation. Ergonomists improve workplace safety. Sports physical therapists guide recovery with data. Motion capture supports all of them.
Different systems have emerged, each suited to a specific way of working. To choose the right one, you need to understand how they operate and what they deliver.
Large-scale productions: optical motion capture
Optical motion capture has long been a standard in film production. Actors perform inside a dedicated capture space, often called a volume stage, wearing markers placed on key body points. Multiple cameras track these markers and send the data into a processing system. You can see this setup in productions like The Lord of the Rings and Planet of the Apes.
This method is known for high accuracy and smooth data. With multiple camera angles, markers remain visible, which helps reduce gaps during editing. Combining footage from all cameras results in detailed animation that holds up in close-up shots.
Markers can be adjusted depending on the level of detail required. More markers mean more precision, especially for facial or fine body movements. Optical systems also support multi-actor capture, making them suitable for crowd scenes where interaction matters.
However, this setup depends on controlled environments, space, and equipment.
Markerless tracking: AI motion capture
AI motion capture removes the need for suits or markers. A single camera can be enough, although multiple cameras improve results. Setup is simple, which makes it appealing for those new to motion capture.
This approach is widely used across industries. Retail uses it for virtual try-ons. Healthcare explores it for rehabilitation. Many consumer applications already rely on it in some form.
The strength of AI motion capture is accessibility. It lowers the barrier to entry and allows quick experimentation. At the same time, accuracy and consistency can vary. For projects that require reliable data, other systems may offer more control.
Versatility and portability: inertial motion capture
Inertial motion capture sits between optical and AI systems. Sensors are attached to the body, either in a suit or as individual units. No cameras are required. Data is processed directly through software.
This setup allows motion capture in almost any environment. From ergonomics studies to game and film productions, users can capture movement without being tied to a studio. Tight spaces, outdoor locations, or complex environments are no longer a limitation.
Xsens inertial motion capture extends this flexibility with magnetic immunity. This built-in capability reduces interference from surrounding environments, helping maintain stable and accurate data. The result is clean motion capture with minimal post-processing.
Professionals benefit from faster setup, fewer constraints, and consistent output across use cases.

Which motion capture system is right for you
Each system has strengths. The right choice depends on what matters most in your workflow.
Consider three key factors:
-
Time, how fast you can set up and capture
-
Accuracy, how clean and reliable the data is
-
Budget, how much equipment and space you need
Optical systems deliver high-end precision in controlled environments. AI motion capture offers accessibility and speed. Inertial motion capture combines strong accuracy with flexibility and ease of use.
For many professionals, inertial motion capture provides a balanced solution. It supports fast setup, delivers high-quality data, and reduces overall production complexity.
Explore what you can create next
If your work demands reliable motion capture without limitations, it is worth exploring inertial systems further. Xsens enables professionals to capture performance anywhere, with consistent data quality and efficient workflows.
Discover how Xsens motion capture fits your workflow.