Motion capture for VFX & Film

With the innovation of Xsens motion capture solutions, both large and small studios can produce animated HQ characters that will keep audiences riveted.

Request pricing

Created to move you

Icon (smaller)

Refined motion engine

Smarter motion from the start with female and male anatomy models, enhanced spine modeling, and proportions.
image (44)

HQ characters, no clean-up

Use raw data to create lifelike, hyperrealistic HQ animations.
image (43)

No limits

Capture clean full-body motion in any environment, inside or out.
Integration icon (small)

Efficient pipeline

Seamlessly integrate with Unreal Engine, Unity, Maya, Motionbuilder, Houdini, and many more – with our plugins.

Easily integrated with Xsens Animate

Supports FBX, BVH, C3D, MVNX exports + plugins for gloves, face, and aiding

Giving you cost-effective motion capture solutions

Two persons on the Love Me set are sitting on a couch displayed on a monitor for BTS

How? By enabling you to record top-quality motion capture data in the most efficient way – without the need for an optical camera set-up.

Request pricing

The most efficient way to animate your characters

MVN-Animate-1-edited

Mocap to go

It doesn’t matter if you’re working on a big-budget summer blockbuster or a small independent film, MVN Animate bundles enable producers to capture motion on the go.

NG-LInk & Animate Resized

Powered by the most advanced motion engine

Xsens delivers high-fidelity mocap through cutting-edge biomechanical modeling, built to capture movement with unmatched realism.

Cardi B 2-edited

From raw to real – fast

Whether you’re bringing a single robot character to life or capturing thousands in a battle scene with a wide shot, VFX artists can quickly turn raw recordings into super-realistic HQ animations. What’s more, you can see recordings on screen in real time.

Productions powered by Xsens

Discover the many famous games that have relied on our motion capture solutions.  

Thanks to the simplicity of the Xsens motion capture suits and set-up,

we could easily capture the fight choreography, get into our rigs, and then start working with cameras in Maya to deliver an early cut."

Scott Meadows
(Head of Visualization)

Survios-Creed-Xsens-1

My team of animators and I have taken the Xsens motion capture system home. We’ve had to do a lot of mocap in our living room,

and the on-body recording also allows us to capture performance in the other parts of the house, like the hallways and stairs, when we need to record climbing or running.”

Han Yang
(CG Supervisor at Method Studios)

Real-Time-Live-–-Kite-_-Lightning-23-edited

…You definitely need a system which is not only robust and dependable but something that is also quite portable and mobile.

Whether it’s running three concurrent characters, delivering dramatic dialogue for a video game cutscene, or high-dynamic stunts in fight scenes – on-set or on-location – we’ve done it all.”

Dave Fialla
(Director and Co-founder of The Mocap Studio)

cinematic-video-prod-greenscreen

One thing that I’m really proud of is that we completed around 400 shots within just 6 months with a small team, but we didn’t have to do any kind of overtime – not a single minute!

Using this motion capture is definitely one of the reasons why we were able to give the artists part of their lives back.”

Claudiua Urban
(Character and Creature Animator at Trixter)

thqnordic-gothic-bts-1-edited

Get in touch

And learn about how Xsens motion capture can be a perfect fit for your application.