Motion capture for Game Development

When it comes to games, we’re not playing around. With Xsens motion capture solutions, studios of all sizes can cost-effectively speed up animation of characters for games and in-game cinematics with inertial motion capture.

Request pricing

Created to move you

Icon (smaller)

Refined motion engine

Smarter motion from the start with female and male anatomy models, enhanced spine modeling, and proportions.
image (44)

Mocap anywhere

Capture character animation in any environment. Indoors or out.
image (43)

Realism, no cleanup

Create realistic movement without the need for data clean-up.
image (45)

Plug and play

The tools you need to instantly stream data straight into Unreal Engine, Unity, Blender, and more.

Easily integrated with Xsens Animate

Supports FBX, BVH, C3D, MVNX exports + plugins for gloves, face, and aiding

Keeping it real

Xsens Avatar in Unreal Engine Jungle

Game characters are always moving. They run, jump, sprint, and hit then do it all again. The instantaneous capabilities of Xsens motion capture solutions make recording new movements simple and realistic.

Request Pricing

With the next generation of Xsens mocap, focus on performance, not technology​

Xsens Avatar hiding in jungle made in UE

Any size, any place

You don’t need cameras and a studio to create convincing animation. Xsens’ motion capture solution allows mocap actors to perform literally anywhere. Developers can then work with motion data, assign this to character rigging, and recreate the motion in-game.

Mocap models posing with avatars in software

Powered by the most advanced motion engine

Xsens delivers high-fidelity mocap through cutting-edge biomechanical modeling, built to capture movement with unmatched realism.

Mocap scene on scaffolding

Reimagine environments

The ability to record motion anywhere means everyday objects in an environment can be utilized in-game. Once users are wearing the suit, chairs can become boulders, walls can become trenches, and so on, eliminating the need to create exact replicas on set. For small and large game developers that need to fine-tune animations, the process is simple and effective.

How Xsens Motion Capture brought Clair Obscur: Expedition 33 to life

A simple punch might be thrown one way in a game, and in another game, the same punch will need to be totally different.”

“Every game has its own ‘action code’ that the performer needs to work within, and that’s what makes the whole process so enjoyable. No game is ever the same.”

Eric Jacobus
(Co-founder of Superalloy)

Mocap actor doing superman punch

Being that the Xsens suit is so versatile and doesn't require an optical set-up, we can record anywhere.”

“For instance, one scene required the actor to jump over a wall. We could just go outside and find a normal wall, rather than having to create an artificial one in the studio.”

Thomas Paul 
(Technical Artist at Iron Harvest)

Gameplay of game made with Xsens mocap

The ability to record anywhere is one of the greatest things about using this technology.”

“In other games, you have to create a motion capture base and bring the actors there. It’s a complicated experience that requires booking long time slots to ensure all the data is recorded. With the Xsens system, we can go straight to the actors in the studio and record directly. We can equip actors with swords and shields and record real fighting.”

Daniel Candil
(Art Director at THQ Nordic)

Mocap model recording mocap data in studio

Xsens allows us to capture an idea and put it in virtual reality in the same day.”

“If we were to use a traditional mocap studio, we’d have to hire a specialized crew, spend time coordinating schedules, and wait a few days for processing and clean-up. It would’ve been too slow.”

John Kim
(Animation Director at Survios)

Mocap model doing face capture

Productions powered by Xsens

Discover the many famous games that have relied on our motion capture solutions.  

Get in touch

And learn about how Xsens motion capture can be a perfect fit for your application.