Press Release

Xsens Helps The Imaginarium Studios Bring the First Real-Time Digital Character to a Shakespeare Performance

Royal Shakespeare Company Stage William Shakespeare’s ‘The Tempest’ in Stratford-Upon-Avon, Featuring Live, Onstage Special Effects

Enschede, The Netherlands – November 18, 2016 – For the first time since its debut in 1611, William Shakespeare’s The Tempest can be seen onstage with all the wonder and magic that the author dreamed of, thanks to a new collaboration between the Royal Shakespeare Company (RSC), Intel and in association with The Imaginarium Studios. The performance includes the first use of a completely digital character in an RSC production, made possible through the use of Xsens’ real-time, MVN motion capture technology.

The Tempest, one of Shakespeare’s final plays, tells the story of Prospero, an exiled magician who decides to settle old scores when his rivals sail past his solitary island. With the help of his magical servant Ariel, Prospero forces the ship to his shores, ready to right old wrongs through magic and cunning. One of the unique parts of Ariel is that the character features more stage directions than almost any other in Shakespeare’s bibliography, making it one of the most complicated to stage.

“For this performance to work, Ariel needed to fly, walk in space and collaborate with other performers in the moment,” said Ben Lumsden of The Imaginarium Studios, the production company founded in 2011 by filmmakers Andy Serkis and Jonathan Cavendish. “Without unrestrictive performance capture technology like MVN, Ariel would have been just another landlocked cast member in a costume.”

During the performance, Ariel morphs from a spirit to a water nymph to a harpy. This transformation is achieved by RSC and The Imaginarium Studios capturing the movements of actor Mark Quartley through Xsens motion capture sensors placed within the actor’s costume. When Ariel transforms into something more than human, the actor’s movements are projected onstage and in the air as a digital avatar. The flexibility of the Xsens technology enables the actor to interact directly with cast members in human form, while being able to transform live on stage every night during the play’s run.

To achieve this transformation, The Imaginarium Studios and the RSC used an Xsens MVN system to track the actor’s performance. The data is run through Autodesk’s MotionBuilder software, and from there into Epic’s Unreal Engine 4. The video output is then sent to d3 servers powered by Intel’s® Xeon® processor connected to the RSC lighting desk, which in-turn controls 27 projectors located around the stage.

“Inertial motion capture is changing how far productions can push their craft, bringing high-end digital characters into live shows,” said Hein Beute product manager at Xsens. “With The Tempest, the RSC is creating a real-time application that is both immediate and novel, something audiences always want to see on their nights out.”

Theater is now entering an era where characters and scenes can be presented in ways that are more visually engaging, and in many cases, far beyond what even the authors originally imagined. Or as Sarah Ellis, the RSC’s head of digital development, told The Guardian in September: “To be able to create digital characters in real time on [this] scale in a theatrical environment is a huge achievement.”

The RSC production of The Tempest runs at the Royal Shakespeare Theatre in Shakespeare’s hometown of Stratford-Upon-Avon. The show runs until January 21, 2017. Tickets are available now at www.rsc.org.uk.

 

About Xsens

Xsens is the leading innovator in 3D motion tracking technology and products. Its sensor fusion technologies enable a seamless interaction between the physical and the digital world in applications such as industrial control and stabilization, health, sports and 3D character animation. Clients and partners include Electronic Arts, NBC Universal, Daimler, Autodesk, ABB, Siemens and various other leading institutes and companies throughout the world.

Xsens has offices in Enschede, the Netherlands and Los Angeles, California. Please contact us on the web at Xsens.

 

######
Xsens and MVN are registered trademarks or trademarks of Xsens Technologies B.V. and/or its parent, subsidiaries and/or affiliates in the Netherlands, the USA and/or other countries.

 

Press Contact:

Liaison Inc.

Heidi Lowell, (503) 796-9822, Heidi@liaisonpr.com
www.liaisonpr.com

 

Xsens Contact:
Remco Sikkema, + 31 88 9736700, Remco.sikkema@xsens.com
www.xsens.com