Blog

Empowering the next generation of creators with the Xsens Academic Program

Studio-grade motion capture, now in the classroom.

For decades, Xsens has set the gold standard in professional motion capture, powering films, games, and virtual productions around the world. With the launch of the new Xsens Academic Program, that same Hollywood-grade technology is now available to schools and universities, giving students and educators direct access to professional tools at an academic scale.

Why motion capture matters for education

Motion capture is not only a production tool, it is a bridge between theory and practice. For educators, it means bringing real-world workflows directly into the classroom. For students, it means gaining the same hands-on experience used in blockbuster films like Marvel’s Black Panther and in popular games like EA’s FIFA.

Unlike optical systems that require costly, dedicated studios, Xsens Animate runs on wireless inertial trackers. Combined with Xsens’ unique magnetic immunity technology, motion capture can be set up in classrooms, labs, performance halls, outdoor areas, or even in the middle of campus. This technology ensures accurate, high-quality data without interference, making mocap anywhere truly possible.

Benefits for educators

The Xsens Academic Program is designed to support institutions where budgets, space, and teaching efficiency are priorities:

  • Flexible licenses of 1, 3, or 5 years for predictable planning
  • Quick setup that makes integration into lessons fast and easy
  • 10 seats with scalable access through network licensing
  • Comprehensive support and resources to help educators get started with confidence

LA Shoot Academic Page imageTrusted by leading universities worldwide. Discover the Xsens Academic Program

Benefits for students

For students, the Academic Program is a direct pathway into the entertainment industry:

  • Hands-on training with the same professional mocap tools used in film and games
  • 100 Record Licenses that let students capture motion inside classrooms, across the school, or even outside on campus grounds and beyond
  • Seamless integration with Unreal, Unity, Maya, Blender, and more
  • Career-ready skills that give graduates a competitive edge when applying to studios and production companies

Next-gen Link mocap shoot (Edu header)Give students access to professional mocap tools with the Xsens Academic Program

Trusted worldwide

Institutions such as California State University, Brigham Young University, Chapman University, Universität Innsbruck, and Georgia State University already use Xsens mocap to strengthen their education. By joining the Academic Program, your school becomes part of a global community preparing the next generation of creators.

CSU-Summers-Arts-7-4Students at California State University bring characters to life with professional mocap. Made possible by Xsens

Start today

The Xsens Academic Program is more than technology. It is a commitment to giving students the tools, skills, and confidence they need to succeed in the entertainment industry.

Apply for the Xsens Academic Program and bring professional-grade motion capture into your classroom.