Customer Case

Breathing Life into a Legend with Xsens Motion Capture

Nestled amidst the quaint towns and rolling hills of England lies the fictional town of Anghenfil, a place where whispers of a long-forgotten legend echo through the cobbled streets. However, the legend is about to become a terrifying reality in Every Legend Ends, a captivating fantasy film written and directed by UK-based filmmaker Ryan Garry.

A Monster Awakens, a Hero Emerges

The film delves into the heart-pounding tale of a monstrous entity, slumbering for centuries beneath the earth. When the creature awakens, its rage unleashes a wave of destruction upon the unsuspecting town of Anghenfil. As fear and chaos grip the community, an unlikely hero emerges, determined to confront the beast and protect their home.

Garry envisioned the film as a high-concept film, drawing inspiration from the epic grandeur of "The Lord of the Rings" and the action-packed thrills of the Marvel Cinematic Universe. However, achieving this level of visual storytelling presented a significant challenge for an independent production.

Xsens Mocap: Breathing Life into the Monster

Behind the scenes: Xsens mocap brings monster vs. soldier fight to life!

Creating a believable monster on screen is no easy feat. It requires careful consideration of both storytelling and technical execution. Garry anticipated challenges in syncing the monster's movements with live-action performers and ensuring realistic and fluid monster movements.

Garry turned to motion capture, and Xsens became the secret weapon for bringing the film to life. Xsens offered the freedom to deploy the technology in various environments, a crucial factor considering the film's diverse shooting locations. From the damp and cavernous depths of Crank Caverns to the historic brickwork of the Williamson Tunnels, Xsens' lightweight and portable design allowed for seamless filming without technical limitations.

The nature of the production needed efficient use of time and resources. With quick and easy setup, Xsens' self-powered system eliminated the need for bulky generators or cumbersome electrical setups, enabling the crew to work efficiently and capture scenes swiftly, even in remote locations.

Unlike optical motion capture that requires separate recordings and post-production adjustments, Xsens allowed for simultaneous capture of the monster and live-action actors on set. This resulted in seamless interaction between the characters, enhancing the film's realism. A prime example is the thrilling fight scene between the monster and an armed response soldier, where Xsens' real-time capabilities eliminated the need for extensive post-production work.

Capturing the nuances and complexities of the monster's movements, especially during fast-paced fight scenes, was crucial for creating a believable creature. Xsens mocap's accuracy ensured smooth and natural movements.

The system's precision minimized the need for extensive post-production adjustments, saving valuable time and resources. The high-fidelity mocap data ensured the monster's movements appeared natural and believable, significantly contributing to the film's immersive experience.

Every Legend Ends stands as a testament to the power of imagination and the ability of Xsens mocap technology to empower independent filmmakers. By embracing this cutting-edge technology, Garry has defied the limitations of independent production and crafted a visually stunning and captivating film, proving that even with limited resources, one can breathe life into a captivating story and create a truly immersive cinematic experience.

The film is expected to be released later this year.  Here is the trailer: