AI is changing how motion can be captured from video. But the right workflow still depends on the performance and production needs.
Markerless motion capture uses cameras, computer vision, and AI to estimate a performer’s movement without attaching optical markers to the body. In the entertainment industry, the term usually refers to video-based systems that turn recorded footage into 3D animation data. Some platforms can work from a single camera, including footage captured on a webcam or smartphone.
This makes markerless mocap an accessible option for early animation tests, previs, education, quick experiments, and projects where performers need to move without wearing a suit. It can also help smaller teams explore an idea before committing more production resources.
The tradeoff is that the result depends on what the camera can see. Body parts may become hidden during turns, floor work, close interaction, or movements where arms and legs cross. Lighting, clothing, framing, image quality, and the type of movement can also affect the final data.
For simple performances, a single-camera workflow may be enough. More demanding scenes may require a more controlled setup.
Adding cameras gives a markerless system more viewpoints. This can improve coverage, support 3D reconstruction, and reduce the effect of joints being hidden from one angle. It does not automatically guarantee better motion data. Camera position, angle, calibration, synchronization, and the software processing the footage all matter.
A 2026 study of a multi-view markerless system found that performance was highly sensitive to camera geometry. A well-positioned stereo pair produced stronger results than less suitable camera arrangements. For a production team, this means that better results may require more than placing extra cameras around a performer.
The setup may also need suitable lenses, consistent lighting, enough capture space, reliable synchronization, calibration, and time to process or clean the data. Markerless mocap can remain cost-effective, especially when standard cameras are already available.
However, the practical cost and complexity can grow as the production asks for more coverage, more performers, faster movement, or fewer visual obstructions.
Xsens inertial motion capture takes a different approach. Wearable inertial sensors measure the performer’s movement directly and send that information to Xsens software, which reconstructs the performance as 3D motion.
Because the system does not need a camera to see each joint, performers can turn away, move behind objects, work in tighter environments, or leave a fixed camera volume. This makes inertial mocap useful for location shoots, virtual production, game development, stunt work, and scenes that involve complex full-body action.
It also brings a level of portability that camera-based setups often struggle to match. Because the suit is wearable and does not rely on a dedicated multi-camera volume, teams can capture motion in different environments without rebuilding an entire optical setup each time.
That flexibility matters when production moves beyond a traditional studio. Motion can be captured in rehearsal spaces, production sets, warehouses, training environments, and even outdoor locations such as a beach, depending on the needs of the shoot. For teams that need to go where the performance happens, portability becomes a practical workflow advantage.
Xsens is also markerless in the literal sense because performers do not wear optical markers. Within the industry, however, it is normally described as inertial motion capture to distinguish it from camera-based AI mocap.
The workflow still requires a wearable system and calibration, so it serves a different need rather than replacing every markerless option. Its main value is dependable capture across changing environments, with real-time visualization and data that can move directly into established animation pipelines.
Magnetic immunity also helps teams capture around metal structures and production equipment.
Hollywood actor Terry Notary captured in action on the beach using Xsens Link.
The best choice depends on the job. Single-camera markerless mocap can be a practical starting point for rapid tests, simple performances, or teams that want to create animation from existing footage. Multi-camera markerless systems can provide more coverage, but they also introduce additional setup decisions.
When a production needs repeatable full-body capture, freedom of movement, reliable data across demanding scenes, and the flexibility to work across different locations, inertial mocap becomes a stronger fit.
When a production needs repeatable full-body capture, freedom of movement, and reliable data across demanding scenes, inertial mocap becomes a stronger fit.
The next-generation Xsens Link is designed for this professional workflow. It uses 17 body sensors, supports a wireless range of up to 150 meters, and connects through Wi-Fi 6E for stable real-time streaming. Xsens has also demonstrated a setup process that is approximately 40% faster than the previous-generation Link.
For Actor Capture, data quality was central when creating the animated lead for Lyle, Lyle, Crocodile. Technical Director James Martin explained that Xsens consistently delivered the quality the team needed.
Markerless mocap makes motion capture easier to access. Xsens Link helps professionals take that motion into demanding production pipelines with confidence.