Real-time Kinematic Positioning
About our RTK
In addition to our other GNSS/INS products, we offer a GNSS/INS module that features an integrated Real-Time Kinematic (RTK) GNSS receiver. Using RTK makes the position estimate of the GNSS receiver more accurate. By using RTK, you can improve your positional data from meter-level accuracy to centimeter-level accuracy. The added benefit of an external RTK model is that it can handle and process high-accuracy position data from external receivers.
Solving unknowns to mitigate error
With standard GNSS, a variety of error sources can cause significant inaccuracies in the estimated position of the receiver. This is because the GNSS uses the estimation of the pseudo-range between satellites and receivers to determine the receiver’s 3D position on earth. Clock errors between the GNSS satellite and GNSS receiver as small as one microsecond will produce an error of 300 meters. By establishing a GNSS fix with four or more satellites at the same time, an RTK receiver can solve for four unknowns: its 3D position and its clock error with respect to the global time.
Atmospheric delays and inconsistencies distorting the radio signals between receiver and satellite are another source of error in standard GNSS position estimation. An RTK GNSS collects correction information to mitigate these errors.
Related cases
Recommended products
You can recognize the RTK-enhanced modules within our different product series by the ‘8’ in the product number.
I have a question
Thinking if Xsens inertial sensor modules will fit your application? Contact us and our Field Application Engineer will get in touch to see how we can support your project.