A UAV needs to know more than whether it is moving. Depending on the application, it may need to know how it is moving, which way it is pointing, where it is and how fast its position is changing.
That is where the distinction between an IMU, AHRS and GNSS/INS becomes important.
These technologies are closely related, but they solve different parts of the navigation problem. Choosing between them is therefore not simply a matter of selecting the most advanced sensor. The right choice depends on what information the aircraft needs and where sensor fusion takes place within the UAV architecture.
A useful way to start is with three questions:
An IMU, AHRS and GNSS/INS answer these questions at different levels.
An Inertial Measurement Unit (IMU) measures the motion of the aircraft using accelerometers and gyroscopes. Depending on the module, magnetic-field measurements may also be available.
The primary outputs are measurements such as:
An IMU does not inherently tell the system its absolute position. Raw inertial measurements also do not directly provide a complete orientation solution without further processing.
Instead, the measurements are typically passed to a flight computer or another processor that runs its own estimation or sensor-fusion algorithms.
When does an IMU make sense on a UAV?
An IMU is a good fit when the UAV already has the processing architecture required to calculate attitude or navigation states.
For example, the flight controller may combine IMU measurements with GNSS, barometer, magnetometer, vision or other sensor inputs within its own estimator.
This gives the development team control over the complete sensor-fusion architecture.
Typical uses include:
The important point is that an IMU provides the measurements used to calculate the aircraft state, rather than the complete navigation state itself.
If the flight computer already performs this processing, adding another complete navigation solution may be unnecessary.
An Attitude and Heading Reference System (AHRS) takes inertial sensing one step further.
Instead of providing only motion measurements, an AHRS uses sensor fusion to estimate the orientation of the platform. Its outputs typically include:
This means another system can use orientation directly without having to derive it from raw accelerometer and gyroscope measurements.
That can be useful when the requirement is not primarily to determine the aircraft's global position, but to know precisely how the aircraft or a payload is oriented.
Where is an AHRS useful?
Typical applications include:
Consider a UAV carrying a stabilized camera.
The payload may not need to know the complete navigation solution calculated by the aircraft. It may simply require reliable roll, pitch and heading information so it can compensate for aircraft movement and maintain the required pointing direction.
An AHRS can provide that information directly.
It can also continue providing orientation when GNSS is unavailable because the orientation solution is not dependent on GNSS position alone. However, an AHRS should not be confused with a complete navigation system: it does not by itself provide an absolute position solution for the UAV.
Once the UAV needs to answer, “Where am I?” as well as “How am I moving?” and “Which way am I pointing?”, the architecture moves toward a GNSS/INS.
A GNSS/INS combines satellite-based positioning with inertial measurements and sensor fusion.
Typical outputs include:
GNSS and inertial sensing complement each other.
GNSS provides an external absolute position reference. Inertial sensing provides continuous, high-rate information about the aircraft's movement between GNSS updates.
The sensor-fusion algorithm combines these sources into one navigation solution.
When should a UAV use a GNSS/INS?
A GNSS/INS becomes relevant when position is part of the actual mission rather than simply another input available to the flight controller.
Examples can include:
It can also help maintain navigation continuity during temporary degradation or interruption of GNSS.
When GNSS measurements disappear, the inertial system can propagate the navigation solution using the last reliable state and subsequent motion measurements.
But there is an important limitation: inertial dead reckoning accumulates error over time.
A GNSS/INS therefore should not be interpreted as providing indefinitely accurate positioning without GNSS. As the period without external aiding increases, position uncertainty also increases.
The required performance during a GNSS interruption should therefore be evaluated against the expected duration, aircraft dynamics and other aiding sensors available on the UAV.
An RTK GNSS/INS builds on the same GNSS/INS architecture but adds Real-Time Kinematic positioning.
RTK uses correction data to improve the GNSS position solution. When suitable correction data and GNSS conditions are available, this can provide centimeter-level positioning.
This becomes relevant when position accuracy directly affects the quality of the UAV mission.
Typical applications include:
For a UAV whose main requirement is stabilization or attitude control, RTK may add little value.
For a mapping or surveying platform, however, precise and repeatable absolute positioning can be a key requirement.
RTK does not replace the inertial part of the system. The INS still provides high-rate motion and attitude information, while RTK improves the absolute GNSS position when correction data is available.
The key question is therefore whether centimeter-level absolute positioning materially improves the mission result.
A Dual Antenna RTK GNSS/INS adds a second GNSS antenna to the RTK GNSS/INS architecture.
Using the known baseline between the two antennas, the system can determine GNSS-based heading. This provides a heading reference without depending on magnetic measurements or requiring forward motion.
That can be especially useful when the UAV is stationary, hovering or moving slowly.
When does dual antenna heading add value?
Dual antenna GNSS becomes relevant when accurate heading is important at standstill or during slow movement, or when magnetic disturbances make magnetometer-based heading less reliable.
It can also add value when the direction of travel differs from the actual vehicle heading. For UAVs, this can happen in strong wind or during sideslip, where the aircraft may be pointing in one direction while moving along a different track.
Typical applications can include:
Flight in strong wind or sideslip conditions
For example, a UAV may require a reliable heading estimate before take-off, during hover or during a slow transition phase or while flying in crosswind conditions. In these situations, direction of travel alone may not provide an accurate representation of where the aircraft is actually pointing.
A dual antenna system can provide true heading from the relative position of the two GNSS antennas, without depending on forward motion or magnetic heading.
As with RTK positioning, performance depends on the GNSS environment and system configuration. Antenna placement, antenna baseline and satellite visibility therefore need to be considered as part of the integration.
The key question is whether the UAV needs not only precise position, but also accurate heading without depending on forward motion or magnetic heading.
| Sensor type |
Main information provided | Choose it when... | It does not provide by itself |
| IMU | Acceleration and angular velocity | The flight computer performs its own sensor fusion or state estimation | Complete orientation or absolute position |
| AHRS | Roll, pitch and heading |
Direct orientation is needed for the aircraft or payload |
Absolute position and velocity |
| GNSS/INS | Position, velocity and attitude | The UAV needs an integrated navigation solution | Indefinitely bounded position during loss of external aiding |
| RTK GNSS/INS | Position, velocity and attitude with RTK-enabled positioning | High-accuracy, repeatable absolute positioning is required | RTK performance without suitable correction data and GNSS conditions |
| Dual Antenna RTK GNSS/INS | Position, velocity, attitude and GNSS-based heading | Precise positioning and reliable heading are required, including at low speed or standstill | Reliable GNSS-based heading without suitable antenna geometry and GNSS conditions |
This also shows why there is no universal hierarchy in which one solution is automatically “better” than another.
They provide different levels of information and solve different navigation requirements.
This is one of the most important questions during sensor selection.
Most UAV architectures already contain several sensors. The flight controller may have onboard inertial sensors, while a separate GNSS receiver provides positioning.
That does not automatically mean that another IMU, AHRS or GNSS/INS is unnecessary.
Instead, the development team should look at which system is responsible for producing the final state estimate.
For example, one architecture may use an external IMU and allow the flight controller to perform all sensor fusion.
Another may use an external AHRS to provide a dedicated orientation solution.
A third may use a GNSS/INS as an external navigation source providing already fused position, velocity and attitude information.
For applications that require both precise positioning and a heading reference at standstill or low speed, a Dual Antenna RTK GNSS/INS may be the more appropriate solution.
The decision is therefore as much about system architecture as it is about sensor specifications.
Before selecting a sensor, define:
Answering these questions usually narrows the sensor choice quickly.
Selecting a UAV navigation sensor becomes easier when the decision starts with the required outputs.
If you need motion measurements that will be processed elsewhere, start with an IMU.
If you need roll, pitch and heading directly, consider an AHRS.
If you need position, velocity and attitude as an integrated navigation solution, a GNSS/INS is the more appropriate architecture.
When precise, repeatable absolute positioning matters, an RTK GNSS/INS may be required.
And when the application also needs accurate heading at standstill, during hover or at low speed, a Dual Antenna RTK GNSS/INS may be the better fit.
The next step is to determine the accuracy, update rate, interfaces, environmental performance and integration requirements within that category, and then validate the complete system on the actual aircraft.
Because the right sensor is not simply the one with the most outputs. It is the one that provides the information your UAV architecture and mission actually require.
Online shop
Visit our online shop to view separately sold accessories such as additional cables and antennas.
Resellers and online catalogs
You can also purchase Xsens products via any of our resellers in or near your country or through an online catalog. You can find an overview here.