Xsens celebrates lustrum in the MTR 100

2 Sep 2013

Xsens is listed in the Marine Technology Reporter 100 (MTR 100) of 2013. With new maritime customers added to the Xsens’ customer database in 2013, the position of Xsens in the maritime market has strengthened with respect to last year.

The 4th generation MTi is excellent for integration into many applications, and has proven itself as easy to use in its first 12 months after release. The success of the MTi in maritime applications is partly caused by the high accuracy that allows the MTi to be used as a replacement for larger and more expensive IMUs.

> Got to the MTR 2013


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now