Stallone and De Niro in Xsens MVN suit for movie Grudge Match

In the movie Grudge Match two retired boxers, played by Robert de Niro and Sylverster Stallone, have a thirty years old grudge which hasn't subsided yet. They have an opportunity to get the score even with one last match.

The trailer shows a scene where Stallone and De Niro have to do a motion capture shoot. In this scene you can clearly see they are both wearing the Xsens MVN system underneath their green suit.Stallone3-1024x538

They are wearing the suit because in the background the actual boxing game is showing the motions of Stallone and De Niro in real-time. The data for the game is coming directly from the Xsens MVN motion capture system.

Watch the full trailer here: