EN

MVN Studio Legacy Download

Here you can download the latest version of MVN Studio for Xsens legacy MVN2 products:

  • Xsens MVN (purchased before December 2014)

 

PLEASE NOTE:
MVN Studio 3.5.3 is only available for the legacy Xsens MVN and MVN BIOMECH products (purchased before December 2014).

 

 

MVN Studio

Download MVN Studio 3.5.3
Release date: January 17, 2014
Release highlights:

  • MVN Awinda and MVN BIOMECH Awinda with wireless trackers is supported.
  • Video Reference: Using VLC encoders the video reference data quality has greatly improved.
  • Movie export has been added meaning that the 3D viewport can be exported to file formats .AVI and .M4U.
  • A new plugin for Unity 3D, which allows the animation of models using live MVN Studio data.
Note:
A valid license key is needed to run MVN Studio.

 

MVN Studio – Older Version

Version details: MVN Studio (Pro) 3.5.1

New:
MVN Awinda and MVN BIOMECH Awinda with wireless trackers is supported.

Improved:
Video Reference: Using VLC encoders the video reference data quality has greatly improved.

Added:
Movie export has been added meaning that the 3D viewport can be exported to file formats .AVI and .M4U.
Play and loop selection. It is now possible to play and replay a specific part of MVN data.
A new plugin for Unity 3D, which allows the animation of models using live MVN Studio data.
FBX has a new mode which will export data with a reference skeleton. This makes the importing of MVN data into software programs like MotionBuilder, Maya, Houdini and Unity much more straightforward.

Removed:
Since multiple calibration steps appears to cause poor data quality, it is now only possible to do one basic (N or T) pose, unless specifically activated by the user (not recommended).
Advanced calibration steps (squat and hand touch) have been move to expert calibration – should only be used following advice from Xsens support.

 

Version details: MVN Studio 3.4.1

Bug Fix Release

Fixed MVN Easy Sync in installer
Double clicking .MNV file will open MVN Studio
Fixed functionality of trimming MVN files
Other minor bug fixes

 

Version details: MVN Studio 3.4

MVN Easy Sync:
MVN Studio PRO has been modified to allow easy synchronisation with third party devices, by means of the Awinda Station.
Start and stop recordings, using TTL 0-3.3V via the intuitive user interface.

MVN Tecnomatix Plugin:
MVN Studio PRO data can now be directly streamed to Siemens Jack (7.1) and Siemens Process Simulate Human (10.1)

NEW! – MVN Maya Live Plug-in 1.0:
MVN Maya Live Plug-in for Maya 2013

MVN MotionBuilder Live Plug-in 5.0
MVN MotionBuilder Live Plug-in now supports both MotionBuilder 2012 and 2013

 

Version details: MVN Studio 3.3

Improved Spine Model:
An improved spine model has been implemented to track the spine more precisely. This improvement especially makes a difference in motions when the spine is bent.

Improved Motion Capture Performance:
The motion capture performance has become more consistent since all Fusion Engine filters have been validated.

X-axis Definition:
Now you can define the direction of the x-axis by performing a ‘NosePointInit’. This allows you to align motions to the X-axis.

MVN SDK 3.3:
The MVN SDK features all the functions available in MVN Studio 3.3. More code examples have been added to make it even easier to integrate the MVN technology into your own application. Access to joint angles has also been added.

Hardware Dongle:
A hardware license dongle is available for MVN Studio and plug-ins. This allows you easily switch licenses between computers.

Download release notes MVNS 3.3

 

Version details: MVN Studio 3.1.5

 

MotionGrid Module:
The ‘NosePointInit’ calibration step is more robust, the outcome is now constant.
Real-time performance is now very similar to the processed result.

MotionBuilder plug-in 2012:
This release supports Autodesk MotionBuilder 2012.

Supported platforms:
– MotionBuilder 2012 (win32)
– MotionBuilder 2012 (x64)
– MotionBuilder 2011 (win32)
– MotionBuilder 2011 (x64)

 

Version details: MVN Studio 3.1

 

 

Version details: MVN Studio 3.0

 

 

Version details: MVN Studio PRO 3.0

 

 

Version details: MVN Studio 2.6

 

New Time code and Remote control plug-in:
Plug-in accepting external time code source and ability to remote control MVN Studio

Improved Motionbuilder Plugin:
Supports multiple actor streaming

 

Version details: Moven Studio 2.5

 

Improved Motionbuilder Plugin:
One click setup
Improved data transfer; Higher output quality
Automatic character scaling
Support for MotionBuilder 2009

Moven SDK:
Moven Fusion Engine handles 3D position aiding input in real-time

 

Version details: Moven Studio 2.1

Calibration:
Better feedback quality (now four levels)
More accurate feedback on magnetic disturbance during calibration (color codes).

Recording:
Improved contact point detection; more natural jumping and running movements (less ‘sticking to the ground’ and improved ‘landings’)
Improved ankle, toe and spine kinematics
Pose reset; brings character back to origin

Edit and export functions:
Edit two contact point segments simultaneously
128-step undo-redo system
Copy part of an MVN file and create a new MVN file
Batch export of complete file folders.

 

BETA DISCLAIMER

Xsens invites you to become a tester of pre-release versions of MVN Studio.

Caution!
This in-development version of MVN Studio may be unstable and contain bugs. Your valuable feedback will help us to create the best MVN Studio software possible. Before you start using the software, please be aware that:

  1. Xsens is not responsible for loss or damage of the data pertaining to usage of the Beta Release.
  2. As the Beta versions have not been officially released by Xsens, they may contain errors or inaccuracies and may result in data loss or cause system reliability issues. If such a problem arises, you may need to use the latest stable release to resume normal operations.
  3. Users acknowledge and agree that Xsens offers software “as is” without warranty of any kind. Xsens shall have no obligation to maintain, correct, update, change, modify or otherwise support the software in beta testing.

 

By downloading and/or using beta software from Xsens, you are considered to have read this Beta disclaimer and agreed to its terms.

 


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now