MT Software Suite MTw Awinda

Here you can download the latest version of the MT Software Suite for the MTw Awinda.

MT Software Suite Includes:

  • MT Manager
  • MT SDK with the following software development tools
    • XsensDeviceApi.dll (XDA) – DLL C interface
    • XDA source files – C, C++ wrapper
    • Example source code for MATLAB, DLL C, DLL C++ and shared object
  • Magnetic Field Mapper executable (GUI) and MFM SDK
  • Complete documentation

MT Software Suite – Latest Stable Release

Download MT Software Suite 4.6
Release date: July 12, 2016

No license keys are required for the MT Software Suite.

  • Code Examples for MTw Awinda
  • Matlab Example now supports multiple MTw’s
  • ‘Awinda Monitor’ example now supports the MTw Awinda
  • Documentation updated for MTw Awinda
  • Document available functions of XsDevices
  • Support for Windows 10

Notes:
Click here to download the MT SW Suite release notes 4.6

MT Software Suite – Latest Beta Release

Download MT Software Suite 2019.1.1 (read the Beta Disclaimer)
Release date: May 2, 2019

By downloading and/or using beta software from Xsens, you are considered to have read this Beta Disclaimer and agreed to its terms.

No license keys are required for the MT Software Suite.

Release highlights:

This release is aimed at fully supporting the New MTw Awinda in the MT Software Suite

Improvements

  • Upgrade to MTSS 2019
  • Linux MTSDK installer now contains links to documentation
  • Installation instructions now included for Linux MTSS

Bug Fixes

  • MT manager no longer crashes during long recordings using MTw
    Awinda DK
  • Graphs are now available for Awinda files
  • C-Sharp examples no longer crash for Awinda
  • Data packets returned from onAllLiveDataAvailable and
    onAllBufferedDataAvailable can now be read by Python

Notes:
Click here to download the MTw SW Suite release notes 2019.1.1

MT Software Suite for Linux

MT Software Suite is also available for Linux (requires a 32 or 64 bit Intel PC).
Download the MT Software Suite for Linux 4.6

MT Software Suite for Linux – Beta

MT Software Suite is also available for Linux (requires a 32 or 64 bit Intel PC).
Download the MT Software Suite for Linux 2019.1.1

Firmware Updater

MT Software Suite firmware updater for Windows.
Firmware Updater for Windows

This is the stable Firmware Updater. Using the latest beta-firmware is possible using these instructions


BETA DISCLAIMER

Xsens invites you to become a tester of pre-release versions of MVN Studio.

Caution!
This in-development version of MVN Studio may be unstable and contain bugs. Your valuable feedback will help us to create the best MVN Studio software possible. Before you start using the software, please be aware that:

  1. Xsens is not responsible for loss or damage of the data pertaining to usage of the Beta Release.
  2. As the Beta versions have not been officially released by Xsens, they may contain errors or inaccuracies and may result in data loss or cause system reliability issues. If such a problem arises, you may need to use the latest stable release to resume normal operations.
  3. Users acknowledge and agree that Xsens offers software “as is” without warranty of any kind. Xsens shall have no obligation to maintain, correct, update, change, modify or otherwise support the software in beta testing.

 

By downloading and/or using beta software from Xsens, you are considered to have read this Beta disclaimer and agreed to its terms.


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now