MT Software Suite Download for MTw Awinda

Here you can download the latest version of the MT Software Suite for the MTw Awinda.

MT Software Suite Includes:

  • MT Manager
  • MT SDK with the following software development tools
    – XsensDeviceApi.dll (XDA) – DLL C interface
    – XDA source files – C, C++ wrapper
    – Example source code for MATLAB, DLL C, DLL C++ and shared object
  • Magnetic Field Mapper executable (GUI) and MFM SDK
  • Complete documentation

MT Software Suite – Latest Stable Release

Download MT Software Suite 4.6
Release date: July 12, 2016

No license keys are required for the MT Software Suite.

Release highlights:

This release is aimed at fully supporting the New MTw Awinda in the MT Software Suite

  • Code Examples for MTw Awinda
  • Matlab Example now supports multiple MTw’s
  • ‘Awinda Monitor’ example now supports the MTw Awinda
  • Documentation updated for MTw Awinda
  • Document available functions of XsDevices
  • Support for Windows 10

Notes:
Click here to download the MT SW Suite release notes 4.6

MT Software Suite – Latest Beta Release

Download MT Software Suite 4.7.2
Release date: April 11, 2017

No license keys are required for the MT Software Suite.

Release highlights:
This release is aimed at fully supporting the New MTw Awinda in the MT Software Suite

Improvements

  • Extended buffering of 90 seconds (typical value)
  • Ability to configure timeout
  • Ability to lock MTw’s to a specific Awinda station

Bug Fixes

  • Fixed bugs in relations to recording length, sync pulses and flushing
  • MTw2 orientation reset now is included in .mtb file using MT Manager
  • Filter init is included when reprocessing MTw2 data in XDA

Notes:
Click here to download the MTw SW Suite release notes 4.7.2

MT Software Suite for Linux

MT Software Suite is also available for Linux (requires a 32 or 64 bit Intel PC).
Download the MT Software Suite for Linux 4.6

MT Software Suite for Linux – Beta

MT Software Suite is also available for Linux (requires a 32 or 64 bit Intel PC).
Download the MT Software Suite for Linux 4.7.2

Firmware Updater

MT Software Suite firmware updater for Windows.
Firmware Updater for Windows 4.0.8

This is the stable Firmware Updater. Using the latest beta-firmware is possible using these instructions.


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now