#!/bin/bash
#
#
# Uninstall script for Sentinel LDK Runtime Environment
#
# return codes:
#   0 - success
#   1 - missing permissions (must be run as root)
#   4 - unrecognized system
#   6 - uninstall aksusbd RPM/DEB failed
#   8 - unsupported hardware platform

# check for root user
if [ `id -u` -ne 0 ]; then
    echo "Installer must be run as root" 1>&2
    exit 1
fi

# check for Linux
if [ `uname -s` != "Linux" ]; then
    echo "Not running on Linux" 1>&2
    exit 4
fi

# detect hardware platform
ARCH=`uname -m`
case "$ARCH" in
    x86_64)
        ARCHTAIL=_x86_64
        ;;
    i?86)
        ARCHTAIL=
        ;;
    armv7l)
        ARCHTAIL=_arm
        ;;
    aarch64)
        ARCHTAIL=_arm
        ;;
    *)
        echo "Unsupported hardware platform" 1>&2
        exit 8
        ;;
esac

# check if a DEB is already installed
dpkg --help > /dev/null 2>&1
if [ $? -ne 127 ]
then
    dpkg -l aksusbd 2> /dev/null | grep "^ii" > /dev/null 2>&1
    if [ $? -eq 0 ]
    then
        echo "Uninstall .DEB from this system" 1>&2
        dpkg -r aksusbd
        if [ $? -ne 0 ]
        then 
            echo "Uninstall .DEB failed" 1>&2
            exit 6
        fi
        exit 0
    fi
fi

# check if a RPM is already installed
rpm --help > /dev/null 2>&1
if [ $? -ne 127 ]
then
    rpm_name=`rpm -qa 2>/dev/null | grep ^aksusbd | head -1`
    if [ ! -z "$rpm_name" ]
    then
        echo "Uninstall .RPM from this system" 1>&2
        rpm -e aksusbd
        if [ $? -ne 0 ]
        then 
            echo "Uninstall .RPM failed" 1>&2
            exit 6
        fi
        exit 0
    fi
fi

# detect what we have installed
if [ -e /etc/systemd/system/hasplmd.service ]; then
    INIT_SYSTEM=systemd
elif [ -e /etc/init.d/aksusbd ]; then
    INIT_SYSTEM=sysv
    INIT_DIR=/etc/init.d
elif [ -e /etc/rc.d/aksusbd ]; then
    INIT_SYSTEM=BSD
    INIT_DIR=/etc/rc.d
else
    echo "Nothing to do" 1>&2
    exit 0
fi

echo "Stop daemons"
case $INIT_SYSTEM in
sysv|BSD)
    sh $INIT_DIR/aksusbd stop
    ;;
systemd)
    if [ ${ARCHTAIL} != "_arm" ];
    then
        systemctl stop aksusbd hasplmd
        systemctl disable aksusbd hasplmd
    else
        systemctl stop hasplmd
        systemctl disable hasplmd
    fi
    ;;
esac

echo "Remove files"

rm -f /usr/sbin/aksusbd
rm -f /usr/sbin/hasplmd
rm -f /usr/sbin/aksusbd_x86_64
rm -f /usr/sbin/hasplmd_x86_64
rm -f /usr/sbin/hasplmd_armhf
rm -f /usr/sbin/hasplmd_arm64
rm -f /etc/udev/rules.d/80-hasp.rules
rm -f /var/hasplm/init/aksusbd.rc
rm -f /var/hasplm/init/aksusbd.service
rm -f /var/hasplm/init/hasplmd.service
rm -f /var/hasplm/init/aksusbd_x86_64.service
rm -f /var/hasplm/init/hasplmd_x86_64.service
rm -f /var/hasplm/init/hasplmd_armhf.service
rm -f /var/hasplm/init/hasplmd_arm64.service
rm -f /etc/hasplm/templates/*.alp
rm -f -r /etc/hasplm/help

case $INIT_SYSTEM in
sysv|BSD)
    if [ -d /etc/rc.d ]; then
        STARTUP_DIR=/etc/rc.d
    else
        STARTUP_DIR=/etc
    fi
    rm -f $STARTUP_DIR/rc2.d/S23aksusbd
    rm -f $STARTUP_DIR/rc3.d/S23aksusbd
    rm -f $STARTUP_DIR/rc4.d/S23aksusbd
    rm -f $STARTUP_DIR/rc5.d/S23aksusbd

    rm -f $INIT_DIR/aksusbd
    ;;
systemd)
    rm -f /etc/systemd/system/aksusbd.service
    rm -f /etc/systemd/system/hasplmd.service
    ;;
esac

# remove files from legacy installers
rm -f /etc/systemd/system/winehasp.service
rm -f /etc/init.d/aksusbd
rm -f /usr/sbin/winehasp

echo "Done"