EN

XPONENTIAL 2016

Xsens will be exhibiting at XPONENTIAL (formally AUVSI’s Unmanned Systems North America) in New Orleans, USA, May 2-5. Be sure to visit us at booth 427.

The New Standard for Professional UAV and Payload Control

At XPONETIAL Xsens will be showing the new MTi 1-series, designed with the use in drones in the back of our minds. In harsh environments and with many constraints on size, weight and power (SWaP), drones, UAVs and payloads have high requirements on the IMU or AHRS. The MTi 1-series has many features that are derived from the industrial-class MTi 10-series and MTi 100-series. The signal processing pipeline is specifically designed for environments with many vibrations and temperature variations. The experience of Xsens in this field is extremely valuable to get the most out of low-cost, low-power MEMS sensors.

MTi 1-series features:

  • High-frequency signal processing pipeline
  • Specific filter profiles for various (aerial applications)
  • Flexible output (software and hardware) to ensure maximum compatibility with UAV system
  • Synchronization possibilities with GPS

 

MTi 1-series applications

  • Navigation
  • Stabilization
  • Payload Control
  • GNSS Support
  • Autopilot

Meet Xsens at XPONENTIAL.

About XPONENTIAL

AUVSI’s Unmanned Systems is now XPONENTIAL

AUVSI has been the industry’s go-to organization for over 40 years. We are at an exciting inflection point today, where advancements in technology are allowing us to build upon our noble heritage of protecting citizens around the world. XPONENTIAL captures the potential of this industry, and defines AUVSI’s commitment to you – now and into the future. Serving as the intersection for commercial and defense applications, and advancing all domains, XPONENTIAL is committed to serving as your ultimate industry brand experience.

More about XPONENTIAL


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now