EN

The Commercial UAV Show UK 2016

Xsens will be exhibiting at The Commercial UAV Show UK 2016 in London, UK, October 19-20. Be sure to visit us at booth 105.

The New Standard for Professional UAV and Payload Control

UAV Drone - Xsens

At The Commercial UAV Show Xsens will be showing the MTi 1-series, designed with the use in drones in the back of our minds. In harsh environments and with many constraints on size, weight and power (SWaP), drones, UAVs and payloads have high requirements on the IMU or AHRS. The MTi 1-series has many features that are derived from the industrial-class MTi 10-series and MTi 100-series. The signal processing pipeline is specifically designed for environments with many vibrations and temperature variations. The experience of Xsens in this field is extremely valuable to get the most out of low-cost, low-power MEMS sensors.

MTi 1-series features:

  • High-frequency signal processing pipeline
  • Specific filter profiles for various (aerial applications)
  • Flexible output (software and hardware) to ensure maximum compatibility with UAV system
  • Synchronization possibilities with GPS

 

MTi 1-series applications

  • Navigation
  • Stabilization
  • Payload Control
  • GNSS Support
  • Autopilot

Meet Xsens at the Commercial UAV Show.

About The Commercial UAV Show

Celebrating its 3rd year as the original and best UAV event in Europe, The Commercial UAV Show brings together UAV pioneers and technology experts to examine new operational inefficiencies and opportunities across the industry.

More about The Commercial UAV Show


X

Xsens newsletter

Signup today to stay updated on all major Xsens news and developments. Subscribe now