Xsens releases MotionGrid at SIGGRAPH 2010
|
MVN MotionGrid is a position aiding system for Xsens MVN. MotionGrid enables real-time driftless multi-person recording. The portable system can be used indoors and outdoors. With a minimal amount of hardware and quick calibration, MotionGrid is a flexible and cost effective system. Large capture volumes of 20x20m (60x60ft) can be easily realized using the default 9-reader MotionGrid configuration. MVN MotionGrid is based on UWB RF technology and therefore does not require line of sight or special lighting conditions. MVN MotionGrid will be on show at the SIGGRAPH conference (July 27-29, 2010) in Los Angeles (CA) at booth 839. See also www.xsens.com/en/general/motiongrid. | 
|
|