Analysis of vehicle ingress and egress


Introduction

The biomechanics group at Coventry University recently completed an analysis of vehicle ingress and egress for General Motors when they were approached by Shanghai Automotive to undertake a similar, but larger, analysis of their vehicles.

For the General Motor study they used their own optical tracking system. For the study described below they approached Xsens to use the MVN BIOMECH system, in order to measure without occlusion. The primary aim of the study was to determine if MVN BIOMECH could be used with our current method, while measuring kinematics and muscle load during ingression and egression of motor vehicles.

Webinar: Biomechanical Analysis in MATLAB and Simulink

Dr. James Shippen will host a webinar September 27th 2011. In this webinar he will illustrate biomechanical analysis within the MATLAB and Simulink environment.

Methods

Subjects

Seven subjects were selected from the employees of SAIC at the Longbridge site to maximise the variation in anthropometric metrics within the sample.

Measurements

To measure the movements of each of the major segments of the body the subjects wore the Xsens MVN BIOMECH motion capture suit. The movement was sampled at 120Hz.

Experimental Protocol

All of the subjects were instructed to ingress and egress current SAIC production vehicles, simulators of future models and comparable competitor vehicles. The subjects were instructed to:

  • Walk to the vehicle through a distance of approximately 4m
  • Open the door
  • Enter the vehicle and sit in the rear seat
  • Close the door
  • Relax in the rear seat for a duration of approximately 2s
  • Open the door
  • Egress the vehicle
  • Close the door
  • Walk to approximately the starting position

No subject spontaneously reported discomfort or movement restrictions due to the measurement equipment.

Results Analysis

Joint angles were provided as direct output from MVN BIOMECH.

Loads in the muscles were calculated using SAM software and importing C3D data from MVN BIOMECH. SAM software is a musculoskeletal model developed at Coventry University. The loads in the muscles of the back were calculated using an optimisation procedure [1, 2]. The SAM method minimises the objective function of the sum of the squares of the muscles’ activation (defined by muscle force divided by maximal isometric force) subject to:

  • The equality constraints - the torques across the joint due to the muscles equals the torque due to inertial load and externally applied loads
  • The upper inequality constraints – the muscle cannot generate more force than the maximal isometric force
  • The lower inequality constraints – the muscle force cannot be less than zero as the muscle cannot push

Results

Major joint articulation angles were recorded for all of the subjects during ingression and egression of 4 vehicles.

Examples of joint articulations are illustrated in Figure 1, with Figure 2 showing a detailed example of the knee angle.

Ingression and egression of vehicles
Figure 1: Selected joint articulations for Subject ST, during ingression and egression of 4 vehicles.

Knee joint during ingression and egression of vehicles
Figure 2: Knee joint for Subject ST during ingression and egression of 4 vehicles.

Figure 3 shows examples of a subject during ingression (Figure 3A), while seated (Figure 3B) and during egression (Figure 3C). The muscle activity is indicated by the colour of the muscle; a blue muscle has little activity whereas the activity of a red muscle is high.

Conclusions

The results from the biomechanical analysis enabled the quantification of the joint articulations and muscle loadings. These results were compared with the results from a parallel study which recorded the user comfort levels whilst entering and exiting the vehicles. Further studies will be undertaken to establish a correlation between biomechanical metrics and vehicle comfort levels.

This study shows that the Xsens MVN BIOMECH system is suitable for recording biomechanical data during ingression and egression and is capable of providing reliable, clean data in effectively real time.

Dr James Shippen
Biomechanics Research Group
Coventry University
UK

References

1) Shippen J, May B, “Calculation of Muscle Loading and Joint Contact Forces in Irish Dance”, Journal of Dance Science and Medicine, Volume 14 1 pp11-18 2010

2) Shippen J, Sports’ biomechanical data capture and analysis
Chapter 8, Design for Sport ISBN 978-0-566-08859-9 Gower Publishing, 201

Coventry University

Xsens Product:

MVN BIOMECH

Analysis of vehicle ingress and egress

Knee joint during ingression and egression of vehicles

alt

Colour coded mussles actication during ingression of vehicles
Figure 3A: Colour coded muscle activations of one subject, during ingression in 4 vehicles (blue – low muscle activation; red – high muscle activation).

Colour coded mussles actication while seatid in vehicles
Figure 3B: Colour coded muscle activations of one subject while seated, in 4 vehicles (blue – low muscle activation; red – high muscle activation).

Colour coded mussles actication during egression of vehicles
Figure 3C: Colour coded muscle activations during of one subject during egression from 4 vehicles (blue – low muscle activation; red – high muscle activation).