Movement Science Customer Cases


Tuesday, 18 October 2011

Objective Functional Capacity Assessment using Xsens MVN System

IntroductionThe Electrical, Computer and Telecom Engineering group at the University of Wollongong recently completed a study to improve the reliability and repeatability of a functional capacity assessment using inertial sensors through objective measurement of a subject’s performance.... >> Full Story

Thursday, 18 August 2011

Stair climbing: a comparison with an optical tracking device

A portable system for collecting anatomical joint angles during stair climbing: a comparison with an optical tracking device  Jeroen HM Bergmann1,3,§, Ruth E Mayagoitia2; Ian CH Smith31 - Medical Engineering Solutions in Osteoarthritis Centre of Excellence, Imperial College London2... >> Full Story

Thursday, 19 May 2011

Analysis of vehicle ingress and egress

Introduction The biomechanics group at Coventry University recently completed an analysis of vehicle ingress and egress for General Motors when they were approached by Shanghai Automotive to undertake a similar, but larger, analysis of their vehicles. For the General Motor study they used... >> Full Story

Wednesday, 25 August 2010

"Outwalk": a novel protocol for clinical gait analysis based on inertial and magnetic sensors

“Outwalk”, with its high potential, can be spread in a pervasive way in the clinical routine, thanks to its simplicity in measuring kinematics, its precision and accuracy and the speed of reporting data.Motion analysis by means of stereophotogrammetry Although motion analysis based on... >> Full Story

Wednesday, 09 June 2010

Baseball pitchers analysis

On August 2009, 18g Xbus kit from Xsens Technologies B.V. (Enschede, The Netherlands) and a software implementing ISEO, a protocol developed by INAIL Prostheses Centre (Vigorso di Budrio, INAIL), for the functional evaluation of the upper limb was provided to Dr. Porcellini staff... >> Full Story

Thursday, 26 November 2009

Wingsuit flight analysis using the MTi-G

A wingsuit may be defined as a wearable suit constructed from a suitable fabric that is flexible, intimately connected to the body, and designed to maximise either the wearer's freefall time or glide ratio.  They offer humans the unprecedented opportunity to experience flight in much... >> Full Story

Tuesday, 03 March 2009

WearIT@Work Project

Omnidirectional Pedestrian Navigation for First Responders It might be assumed that dead reckoning approaches to pedestrian navigation could address the needs of first responders, including fire fighters. However, conventional pedestrian dead reckoning approaches with body-mounted... >> Full Story

Tuesday, 03 March 2009

Stroke patients

Characterising patterns of muscle activation in stroke patients during walking Stroke affects approximately 100,000 people per year in the UK and can result in long term motor dysfunction. The qualities of differing therapies, to improve motor function, are rarely assessed... >> Full Story

Tuesday, 03 March 2009

Extreme conditions

Mechanics and energetics of loaded walking on gradients:Management of resources in extreme conditions Prof. Minetti of the Institute for Biophysical and Clinical Research into Human Movement coordinated a team of researchers to carry out an evaluation project entitled "Mechanics and... >> Full Story

Monday, 02 March 2009

Racehorse lameness

Fast, accurate and robust detection of lameness of racehorses Lameness of racehorses is assessed at an early stage using 3 MT9s along the spine of the horse. At the trotting track of Cabourg (Normandy, France, see photograph) researchers affiliated with the Cirale measure the symmetry... >> Full Story

Sunday, 01 March 2009

Ergonomics

Human-machine interaction, particularly in the work place is becoming increasingly important. Ergonomic research can now be carried out in the work place on-site, for example, ambulant measurement systems can be taken to assembly lines. The sensors are... >> Full Story

Sunday, 01 March 2009

Wearable assist devices

Inertial motion sensors as building blocks for wearable assist devicesThe miniaturization of electronics has allowed the creation of new biofeedback assistive devices that can be worn on a belt and even embedded into clothing without affecting the wearer's ability to perform normal daily... >> Full Story

Sunday, 01 March 2009

Rowing with MVN

Rowing with MVN   Roessingh Research & Development (RRD), in Enschede, the Netherlands investigates the technological and methodological (im)possibilities of application for coaching in competitive rowing, in collaboration with Dutch rowing clubs of Protheus (Delft)... >> Full Story