EntertainmentMVN (formerly Moven) is a full-body, camera-less inertial motion capture (MoCap) solution. It is flexible motion capture system that can be used indoors or outdoors (on-set). With the short turnaround times MVN is a cost effective system with clean and smooth data. |
> Xsens MVN Customer Examples
________________________________
Previs for X-Men: First Class
The Previs Department of 20th Century Fox and The Third Floor have been working on the previs for 20th Century Fox's X-Men: First Class >
FreeStyle 2 Street Basketball
For this game our distributor Motion Technologies worked on the motion capture files and shot most of moves on an indoor basketball court.>
Insomniac Games: Resistance 3
Kevin Grow, Cinematics Director at Insomniac Games, talks about how the Xsens MVN motion capture system was used in the animation pipeline for Resistance 3 >
Vestel commercial
The robots were animated using Xsens MVN, which enables post-production companies to do many more visual effects in much less time compared to traditional motion capture solutions >
Skrillex: Live on stage!
For his 2011/2012 world tour Skrillex introduced a live motion capture act to his on stage performance using the Xsens MVN mocap suit >
'Paul' the movie
For the feature film ‘Paul’, the Xsens MVN motion capture solution was used by actor Seth Rogen >
Sony Computer Entertainment game: Killzone 2
Guerrilla Games has integrated Xsens MVN into their pipeline for the development of Killzone 2 because of its flexibility and quick turnaround time >