Create PDF Print

When exporting data with the MT Manager, I do not see any data / I do not see the data I expected.


Author:
Xsens Admin
Date added:
Wednesday, 21 July 2010
Last revised:
Wednesday, 21 July 2010

Answer

Please review the exporter settings in MT Manager: Open the Tools menu and select Options, then expand the Exporter tab. Also make sure that the output options of the motion tracker are configured appropriately.

For offline analysis, it may be advantageous to log Raw Inertial data (MTi/MTx) or Raw Inertial & GPS PVT (MTi-G), as these offer the most complete options in post-processing, including reprocessing with different filter scenarios.

Category

Tags for this item