Create PDF Print

Motion Tracker (MTi MTx MTi-G) not recognised at baud rate 9600


Author:
Xsens Admin
Date added:
Wednesday, 09 September 2009
Last revised:
never

Answer

The problem is related to an issue with Windows OS, that may interpret devices communicating at 9600 baud as a pointing device.

The MT Manager or CMT may then not be able to detect the motion tracker. To solve this problem, use the 'Restore Communication' wizard in the MT Manager Tools menu or refer to the procedure described in the section 'Restore Communication' the MT Low-Level Communication Documentation.

If that does not solve the issue, alse refer to the FAQ item 'The Xsens USB converter is detected as a computer mouse.'.

Category

Tags for this item