Create PDF Print

Are wireless solutions available for Xsens motion trackers?


Author:
Xsens Admin
Date added:
Thursday, 23 September 2010
Last revised:
Thursday, 21 July 2011

Answer

Xsens offers a wireless solution with the MTw Development Kit. This is the first completely wireless system from Xsens. Please use the general contact form if you wish further information about the MTw Development Kit.

Additionally, Xsens offers a wireless solution with the Xbus Kit. This provides a wireless connection between the person and the PC. Please use the general contact form if you wish further information about the Xbus Kit.

Our standalone motion trackers (MTi, MTi-G or MTx) feature a standard serial interface (RS232, RS422 or RS485, depending on the model). It is possible to replace the wired link by a wireless connection. Serial to wireless converters are commercially available through various manufacturers and dealers in electronics.


Xsens offers a wireless solution with the MTw Development Kit. This is the first completely wireless system from Xsens. Please see use the general contact form if you wish further information about the MTw Development Kit.

 

Additionally, Xsens offers a wireless solution with the Xbus Kit. This provides a wireless connection between the person and the PC. Please see use the general contact form if you wish further information about the Xbus Kit.

 

Our standalone motion trackers (MTi, MTi-G or MTx) feature a standard serial interface (RS232, RS422 or RS485, depending on the model). It is possible to replace the wired link by a wireless connection. Serial to wireless converters are commercially available through various manufacturers and dealers in electronics.

Category