Is there a USB version of the MTi / MTx or MTi-G?
- Date added:
- Tuesday, 03 March 2009
- Last revised:
- Thursday, 05 March 2009
Answer
By default, all Xsens devices are delivered with an Xsens USB Converter. The USB converter also provides power to the device. The serial communication from a standalone motion tracker to USB Converter can be chosen from RS-232, RS-422 or RS-485. Serial cables with DB-9 connectors and separate DC power connector or a simple Molex connector can be purchased from Xsens.