Create PDF Print

Installation of MVN Studio


Author:
Xsens Admin
Date added:
Tuesday, 28 July 2009
Last revised:
Wednesday, 01 December 2010

Answer

Xsens' MVN Studio is compatible with Windows XP, Windows Vista and Windows 7.

For installation under any Windows OS, being logged in as a user of the administrator group is not sufficient. Start the installation by right-clicking on the installer and selecting 'Run as administrator'.

After installation, run the Software Activation tool to register your license. Refer to the software Acitvation User Manual for detailed instructions.

Xsens (strongly) recommends using an "always on" power scheme when using Windows Vista or Windows 7. Both operating systems implement powersaving features that may affect the performance of the viewports in MVN Studio as well as operation of the WR-As, which are powered by the USB ports. Some of these power saving features may be active in the default power scheme.

Category