In some applications, it can be advantageous to log data with third party hardware or software and later process this data with the MT Manager offline.
For the MT Manager to be able to interpret the data, configuration data and the proprietary EMTS data must be present in the file. The respective two messages are sent by the motion tracker on power-up or after receiving the <Reset> command. Note that EMTS data is only sent at wake-up if the RawData ouput mode is enabled.
Refer to the User Manual for information about the wake-up procedure that is initiated at start-up or by the <Reset> command and to the MT Low-Level Communication Documentation for information on the <Reset> command.