Create PDF Print

Is there a USB version of the MTi / MTx or MTi-G?


Author:
Xsens Admin
Date added:
Tuesday, 03 March 2009
Last revised:
Thursday, 05 March 2009

Answer

By default, all Xsens devices are delivered with an Xsens USB Converter. The USB converter also provides power to the device. The serial communication from a standalone motion tracker to USB Converter can be chosen from RS-232, RS-422 or RS-485. Serial cables with DB-9 connectors and separate DC power connector or a simple Molex connector can be purchased from Xsens.

Category

Training & Simulation , Movement Science , Aerospace , Ground , Marine , Industrial Applications

Tags for this item

Accesories , Hardware , MTi , MTi-G , MTX , XBus Kit