Create PDF Print

How do I work with the motion tracker's scenarios in CMT?


Author:
Xsens Admin
Date added:
Tuesday, 03 March 2009
Last revised:
Tuesday, 03 March 2009

Answer

When using the CMT, you can get a list of all available scenarios using the cmtGetAvailableScenarios function. The cmtGetScenario returns the currently used scenario. You can set the scenario using the function cmtSetScenario. For software filtering, the scenarios are also available in the scenarios.xsb file. You can load them using the cmtLoadScenarios, cmtGetAvailableSoftwareScenarios and other functions that look much like the previously mentioned functions. Also refer to the API function reference.

Category

Tags for this item