Create PDF Print

Why is my Motion Tracker not recognized by MT Manager?


Author:
Xsens Admin
Date added:
Thursday, 21 July 2011
Last revised:
Thursday, 21 July 2011

Answer

The MT SDK contains a driver for the USB to serial converter. It will be installed once you install the MT SDK. If your Motion Tracker is not recognized by MT Manager and a restore communication does not work there could be a problem with the driver.

How do I know if the driver has been installed correctly?

Go to Control Panel and select system –> device manager

Under the tab Universal Serial Bus Controllers the Xsens USB-serial Converter should be listed. If it is not, the driver has not been installed correctly.

Why is the integrated driver not working?

This is a Windows related problem. In some cases the integrated driver will not be installed correctly by Windows and you will not be able to connect to the Motion Tracker.


To solve this, use this link to download a separate driver: www.xsens.com/download/Driver_USB_serial_converter.zip

Category

Tags for this item