Why does the MT Manager not allow to use my motion tracker in sync in mode?
- Date added:
- Wednesday, 24 March 2010
- Last revised:
- Monday, 12 July 2010
Answer
The MT Manager expects data coming in continuously from connected devices. If the device is waiting for an external trigger signal to send data, a timeout will occur. You will need to write your own program to acquire data from a synced MTi. Several preprogrammed examples are installed to your PC as part of the MT SDK. Please refer to the folder <*\Xsens\Software Development\Examples\>.
The next release of the MT SDK will also allow recording with MT Manager using SyncIn modes.