Is the MT SDK compatible with Windows Vista or Windows 7?
- Date added:
- Thursday, 07 January 2010
- Last revised:
- Friday, 08 January 2010
Answer
MT SDK 3.2.4 and earlier are compatible with Windows XP and Vista. The strict security policies under Windows Vista make a careful installation necessary. Please refer to the FAQ item 'Installation of the MT SDK'.
Please appreciate that MT SDK 3.2.4 has not been developed for Windows 7.
Feel free to install MT SDK 3.2.4 on Windows 7. Other customers have successfully installed MT SDK 3.2.4 on Windows 7 OS and are reporting full functionality. Do contact us through the support contact form (http://www.xsens.com/en/contact-form) if you encounter problems with the installation or operation on Windows 7 but keep in mind that support we can provide may be limited.
Xsens also (strongly) recommends using an "always on" power scheme when using Windows Vista or Windows 7. Both operating systems implement powersaving features that may affect the performance of the viewports as well as operation of the WR-As, which are powered by the USB ports. Some of these power saving features may be active in the default power scheme.